Ethernet on i.MX RT 1170

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Ethernet on i.MX RT 1170

403 次查看
gantener
Contributor I

 

I am required to conduct Ethernet debugging on an i.MX RT1170 development board running the RT-THREAD operating system. Within the i.MX RT1170 Processor Reference Manual, I've encountered several Ethernet options: ENET, ENET1G, and ENETQOS. Could you specify which of these is utilized for Gigabit Ethernet operations? It's mentioned that ENETQOS is an Intellectual Property (IP) from Synopsys.

 

here is the open source code

https://gitee.com/rtthread/rt-thread/blob/master/bsp/imxrt/libraries/drivers/drv_eth.c

0 项奖励
回复
2 回复数

388 次查看
xjy198903
Contributor III

ENET1G is used in rt1170 in rt-thread and it is Gigabit Ethernet

0 项奖励
回复

384 次查看
gantener
Contributor I

i want to use ENET_Qos ,Have you adapted under rt-thread? i did not find the code?will you please show me,thanks!

0 项奖励
回复