Hi,
I am using
Board : IMX6 Solo Lite EVK Board
Android : KITKAT 4.4.2
Linux Kernel Version : 3.0.35
When connected to a 100 Mbps network, my network is stable. But when I connect to a 1000 Mbps link, network is very unstable.
On the terminal log I can see: net eth0: FEC ENET: rcv is not +last
I also attached the log.Please find it and suggest to solve this problem
Best regards,
vinothraj
Original Attachment has been moved to: Log.txt.zip
Hi ,
anybody soved this issue?
Regards,
vinothraj
Hi vinothraj
please try enable_wait_mode=off in kernel boot parameter
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor,
Thanks for your quick reply.
I added the enable_wait_mode=off in kernel boot parameter and boot it.
But it does not work.
I connect to a 1000 Mbps link, network is very unstable still.
On the terminal log I can also see: net eth0: FEC ENET: rcv is not +last
To solve this by adding any patches to .../myandroid/kernel_imx/drivers/net/fec.c ?
Best regards,
vinothraj