Hi all.
I want to use kernel 4.1.15 BSP.
so i upgrade 3.0.35 LTIB -> 4.1.15 YOCTO . It is success for mount on i.mx6 solo sabresd board.
But do not run ping...
I was set below...
# ifconfig eth0 192.168.17.11 up <== my sabresd board ip.
eth0 Link encap:Ethernet HWaddr 5e:c9:69:76:94:b3
inet addr:192.168.17.11 Bcast:192.168.17.255 Mask:255.255.255.0
inet6 addr: fe80::5cc9:69ff:fe76:94b3/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:678 errors:0 dropped:0 overruns:0 frame:0
TX packets:493 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:88207 (86.1 KiB) TX bytes:44150 (43.1 KiB)
It's OK.
BUT when input command below..
# ping 192.168.17.10 <== my pc ip.
PING 192.168.17.10 (192.168.17.10): 56 data bytes
it's then. stop.
-----------------------------------------------------------------------------------------------------------
compare i.mx6dl sabresd board. ( I have two board : i.mx6 solo sabresd board , i.mx6dl sabresd board)
Same kernel and files(rootfs , dts , zimage etc...) accept.
# ping 192.168.17.10 <== my pc ip.
64 bytes from 192.168.17.10: seq=0 ttl=64 time=1.724 ms
64 bytes from 192.168.17.10: seq=1 ttl=64 time=0.687 ms
64 bytes from 192.168.17.10: seq=2 ttl=64 time=0.586 ms
64 bytes from 192.168.17.10: seq=3 ttl=64 time=1.323 ms
64 bytes from 192.168.17.10: seq=4 ttl=64 time=0.453 ms
Oh.. my god.. it's run..!!
OTL...
Why does i.mx6dl sabresd work on the Ethernet ping?
I want to work on i.mx6solo board ethernet ping....!!!
Why are the two machines operating differently?
If do you have soloution.. please share for me..
Hi Hanseung,
As there is no eval board with IMX6S I am assumning you refer to IMX6SX-SABRESD board, which has dual Ethernet ports, Right?
Please note that only one of the Eth ports is defined, you can check in /etc/network/interfaces file if it is defined properly. You can also enable the 2 ports. You may try first with static IP by adding the information below in /etc/network/interfaces.
For a DHCP client:
auto eth1
iface eth1 inet dhcp
For a Static IP (of course this is an example, your numbers will be different):
auto eth1
iface eth1 inet static
address 192.168.0.100
network 192.168.0.0
netmask 255.255.255.0
broadcast 192.168.0.255
gateway 192.168.0.1
Regards,
Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------