Ethernet Setting ( Static - IPV4) is not getting stored on i.MX8QM MEK board running on Android 13.0.0_2.0.0 (L6.1.22_2.0.0 BSP). I am not getting any error message while configuring the IP address of the evaluation board. The behaviour is same on i.MX8M plus board too.
Configuration of IP address using Ifconfig command is not persistent. Configuration get lost after reset on even on plug unplug network cable.
Ethernet APK has been also removed from android 13 prebuild image.
Please help to getting it resolve.
Thanks in advance.
Sanjay Pandey
Hi @Sanjay_Pandey1,
Thank you for contacting NXP Support.
In this case you can try adding a script to the init.rc file, configuring your static IP address.
Here is a link to an article describing the init.rc file and how to use it.
What is inside the init.rc and what is it used for... - NXP Community
Have a wonderful day!
Hi @Sanjay_Pandey1,
Yes, init.rc is called during the boot process after the kernel initialization.
Regarding the ethernet app for Android 13, I will review in the next Android release if this app can be included.
Have a great day!