Ethernet Setting is not getting stored on Android 13 [i.MX8QM MEK Board]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet Setting is not getting stored on Android 13 [i.MX8QM MEK Board]

1,902 Views
Sanjay_Pandey1
Contributor II

Ethernet Setting ( Static - IPV4) is not getting stored on i.MX8QM MEK board running on Android 13.0.0_2.0.0 (L6.1.22_2.0.0 BSP). I am not getting any error message while configuring the IP address of the evaluation board. The behaviour is same on i.MX8M plus board too.

Configuration of IP address using Ifconfig command is not persistent. Configuration get lost after reset on even on plug unplug network cable.

Ethernet APK has been also removed from android 13 prebuild image.

Please help to getting it resolve.

Thanks in advance.

Sanjay Pandey

 

 

 

 

 

 

 

 

0 Kudos
Reply
4 Replies

1,845 Views
brian14
NXP TechSupport
NXP TechSupport

Hi @Sanjay_Pandey1

Thank you for contacting NXP Support.

In this case you can try adding a script to the init.rc file, configuring your static IP address.

Here is a link to an article describing the init.rc file and how to use it.

What is inside the init.rc and what is it used for... - NXP Community

Have a wonderful day!

0 Kudos
Reply

1,794 Views
Sanjay_Pandey1
Contributor II
Hi Brian Ibarra,
Thanks for your quick response , I will try the same and let you know whether it works for me or not. As per my understanding init.rc will be called during boot time of the device where as network configuration setting also getting lost in case of network cable plug/unplug. How to handle this plug/unplug issue while device is in running state.

Is there any specific reason why this ethernet app has removed from prebuiled image of Android 13 without getting validated inbuilt ethernet setting option ?

Thanks & Regards,
Sanjay Pandey


0 Kudos
Reply

1,563 Views
brian14
NXP TechSupport
NXP TechSupport

Hi @Sanjay_Pandey1

Yes, init.rc is called during the boot process after the kernel initialization.

Regarding the ethernet app for Android 13, I will review in the next Android release if this app can be included.

Have a great day!

1,552 Views
Sanjay_Pandey1
Contributor II
Hi Brian Ibarra,
Thanks for your valuable response.

Thanks & Regards,
Sanjay Pandey
0 Kudos
Reply