Please see the attached file for detail Picture : Ethernet MII mode issue on i.MX8MM_wKSZ8081MNX_20190904.pptx
* Applied IC
1) Applied CPU : i.MX8MM (MAC included, possible RGMII/MII)
2) Applied PHY IC : KSZ8081MNX (Only MII mode)
1. Symptom
A) ping communication between [PHY]-[MAC] is impossible (MAC setting : MII mode)
Picture A.1) : when connecting <TXC line> between [PHY]&[MAC] measuring <TXC line>
Picture A.2) : when cutting <TXC line> between [PHY]&[MAC] and measuring <TXC line > of PHY side.
Picture A.3) : when cutting <TXC line> between [PHY]&[MAC] and measuring <TXC line > of MAC side.
>> 25MHz Clock comes out from PHY side, Clock does not come out from MAC,
Voltage level decreases when connected to each other
B) Ping communication between [PHY]&[MAC] is possible, but sometimes disconnection(MAC setting: RGMII)
Picture B.1) when connecting <TXC line> between [PHY]&[MAC] measuring <TXC line>
>> 25MHz clock comes outboth PHY & MAC
So, Ping communication seems sometimes possible because the signal is overlapped,
but there is a disconnection depending on the voltage level.
2. Review for RGMII vs MII
1) RGMII : TXC(TxClock) go to from [MAC] to [PHY]
2) MII : TXC(TxClock) go to from [PHY] to [MAC] > Our Case
3. Symptom prediction
1) We suspect the setting for“ENET_TXC“ net(Ball no.: AG24) of i.MX8MM for MII modeseems to be wrong.
4. Request
1) please sharea patch or SW guide for MII mode.
2) please share the HW guide for MII mode.
Hi Lee
unfortunately i.MX8M Mini MII mode is not supported in NXP BSPs, no
software examples are available. Recommended to proceed with extended support
of Commercial Support & Engineering Services | NXP for developing patches.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor,
[i.MX8M Mini] can support "MII mode" like below (IMX8MMRM.pdf > Page 3673)
Request) We're appreciated if NXP team guides for the use of "MII mode".
PS) If [i.MX8M Mini] has a difficulty to support "MII mode", please explain the reason.
Thank you.
BR / Ken
Hi
recently I got update below:
-------------
After confirm with SOC team, both MII and MIILite are not supported by i.MX 8M-Mini.
RM will be updated later.
-------------
sorry for confusion.
Best regards
igor
Hi Lee
yes hardware supports it, but unfortunately i.MX8M Mini MII mode is not supported in
software - NXP BSPs, because there is no reference board with MII configuration.
For that reason recommended to proceed with extended support
of Commercial Support & Engineering Services | NXP for developing patches.
Best regards
igor
I''m Ken Lee
who posted above question for "Ethernet MII mode issue on i.MX8MM (Applied PHY IC : KSZ8081MNX)"
I'm posting additional SW review like below.
1. Review : SW Changes for [RGMII (default) to MII mode]
* Operating Environment: u-boot Status (not Kernel Status)
1) To Change Parameter in “imx8mm_evk.h”
>Before : #define CONFIG_FEC_XCV_TYPE RGMII
> After : #define CONFIG_FEC_XCV_TYPE MII100
2) To Check “register setting value change.
(Related Register map & SW code like below)
> Before
(1) FEC_RCNTRL_FCE 1
(2) FEC_RCNTRL_MII_MODE 1
(3) FEC_RCNTRL_RGMII 1
> After
(1) FEC_RCNTRL_FCE 1
(2) FEC_RCNTRL_MII_MODE 1
(3) FEC_RCNTRL_RGMII 0
2. Request
1) Please share if additionally Register settings or additional works are required for the use of MII mode.