Enter Recovery Mode Through JTAG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enter Recovery Mode Through JTAG

872件の閲覧回数
romanschnarwile
Contributor III

Is it possible to enter recovery mode on i.MX6 Solo and DualLite through some JTAG commands. I'm looking for the easiest way possible, as we plan to use a bit-bang JTAG approach without  any predefined configuration files, etc like would be available on e.g. Lauterbach. I'm thinking about a simple IR and DR combination to modify the GPR9 and 10 register. Or a simple way of loading a small assembler code into internal ram and execute this. Any solution is OK as long as it can be done through JTAG only.

We would like to enter recovery mode on a device where the HW recovery mode (BOOT_MODE0) pin isn't available.

We just started looking at this, so any input or suggestion might be helpful.

Thanks.

Roman

Toradex

ラベル(2)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

632件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Roman

suggest to look at link

Use JTAG to force entry into Serial Downloader mode

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

632件の閲覧回数
romanschnarwile
Contributor III

Hi Igor,

Thanks. I didn't find that post. Looks promising, we'll l give it a try. I try to update this post here with our findings, but give me some time.

Have a nice weekend

Roman

0 件の賞賛
返信