iMX6 solo: LVDS pixel clock looked up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 solo: LVDS pixel clock looked up

996 Views
beatgaehler
Contributor I

I'm working with i.MX6 solo processor and I conect a LVDS panal to the board. Sometimes the LVDS clock is not generated by the processor.

I change the clock base from the default setting MMDC_CH1 clock to the pll5 clock to set the needed clock frequency.

Is there a problem with the LVDS clock generator if I change the base clock?

Can somebody help me?


Labels (4)
0 Kudos
Reply
3 Replies

578 Views
igorpadykov
NXP Employee
NXP Employee

Hi Beat

one can test LVDS clock with SDK and check if it is caused by

HW or SW reasons

i.MX 6Series Platform SDK : Bare-metal SDK for the i.MX 6 series

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

578 Views
beatgaehler
Contributor I

Hello Igor

Thank you for the fast answer but I could not solve the problem.

I found the following description from Ranjani.Vaidyanathan freescale.com and fabio.estevam freescale.com:

[PATCH] ARM: imx6: Fix procedure to switch the parent of LDB_DI_CLK

I have a Windwos Embedded Compact 7 environment so I adapted the linux code to my boot code. But it's not working!

I also tried to change only the frequence of the MMDC_CH1_AXI_CLK_ROOT but without success.

Do you have contact to this person above to get more information about the behavior of the ldb_di_ipu_divider?

I can reboot the CPU between 10 to 300 times and then the ldb_di_ipu clock is not working!

Kind regards

Beat

0 Kudos
Reply

578 Views
igorpadykov
NXP Employee
NXP Employee

Hi Beat

some of them working on meta-fsl-arm mailing list:

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

igor

0 Kudos
Reply