Eink play video issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Eink play video issue

660 Views
张松源
Contributor III

hello,
    our product parameter as blew:
    chip : imx6sl
    sw system : android 4.4.0
    screen : Eink  resolution is 1872X1404
    I try to change system update display mode, set WAVEFORM_MODE_ANIM and EPDC_FLAG_USE_DITHERING_Y1 when play a video.but the effect is no good.
    please check the effect video in attachment.

     please give me some advice, make the video play fluent。 thank you!!

best regard!

Labels (1)
Tags (1)
0 Kudos
3 Replies

514 Views
igorpadykov
NXP Employee
NXP Employee

Hi

i.MX6SL has not VPU and video performance is not high, it is described in

Table 10. Video Codec Specification attached Release Notes (android 4.4

is based on linux L3.0.35).

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

514 Views
张松源
Contributor III

hi igorpadykov

  The sliding effect of the interface also not good, Is it related to the screen resolution?

  is there anyway can reduce the display effect to increase sliding effect?

 best regard!

0 Kudos

514 Views
igorpadykov
NXP Employee
NXP Employee

Hi

please check typical performance in Table : it is about D1@30fps.

Best regards
igor