Ecran clavier non reconnus au démarrage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ecran clavier non reconnus au démarrage

613件の閲覧回数
pascalmarestin
Contributor I

Bonjour,

Premier essai de la board IMX7 SABRE (dual appli duo), sur laquelle je boote simplement sur la carte SD fournie (Linux L4.1.15_2.0.1) je branche un ecran LCD (port HDMI) et un clavier (port USB). L’écran n'est pas reconnu ni le clavier .

J'obtiens une trace par le port de debug qui semble confirmer un problème de driver video.

Ensuite forcément, sans clavier impossible d'aller plus loin.

Des idées ? Je pensais qu'il n'y avait rien de particulier à faire pour un tel essai "out of the box"

Merci

pascal

ラベル(1)
0 件の賞賛
2 返答(返信)

466件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Pascal,

From the log you shared the bootloader is not finding any panel and defaulting to the TFT43AB.

If you wish to use HDMI for display output you would need to add the corresponding boot arguments. You may find them on the i.MX Linux Release Notes. They would be:

video=mxcfb0:dev=hdmi, 1920x1080M@60,if=RGB24

You would need to add these variables using the debug console.

I hope this helps!

Regards,

0 件の賞賛

466件の閲覧回数
pascalmarestin
Contributor I

Hello,

Thanks for your answer, but this does not work.

The main problem is not the screen, since I can see the boot sequence through the console

I connect a laptop with minicom installed.

And I use the supplied USB cable to connect to Debug UART port)

I see that the linux OS is started and when the “login :” is displayed I m not able to enter anything.

Neither trying with a keyboard on the USB port nor trying through the console interface

I think a correctly follow instructions from SABRE Board QSG, but something goes wrong

And when I look at the console I can see

“hid-generic 0003:17EF:6007.0001: input: USB HID v1.10 Keyboard on usb-ci_hdrc.1-1/input0

hid-generic 0003:17EF:6007.0002: device has no listeners, quitting

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver”

I don’t know if it is a normal behavior.

Any idea ?

I wish you an happy new year,

Regards,

Pascal

De : gusarambula

Envoyé : vendredi 29 décembre 2017 00:00

À : MARESTIN Pascal

Objet : Re: - Re: Ecran clavier non reconnus au démarrage

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Ecran clavier non reconnus au démarrage

reply from gusarambula<https://community.nxp.com/people/gusarambula?et=watches.email.thread> in i.MX Community - View the full discussion<https://community.nxp.com/message/973230?commentID=973230&et=watches.email.thread#comment-973230>

0 件の賞賛