ETH_VDDIO on SabreSD i.MX6 Quad EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ETH_VDDIO on SabreSD i.MX6 Quad EVK

664 Views
vincentchou
Contributor IV

Dear support,

Based on the i.MX6 EVK schematic, ETH_VDDIO should be 1.8V or 2.5V.  Unfortunately we accidentally wired 3.3V to ETH_VDDIO to NVCC_RGMII on our board.  Luckily we don't use any Ethernet components on our board.  I would like to ask your opinion whether this voltage will cause problem of the operation of the board and the CPU?

Vincent

Labels (4)
0 Kudos
Reply
1 Reply

607 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vincent

i.MX6Q max. NVCC_RGMII  is 2.625V according to Table 6. Operating Ranges

Table 6. Operating Ranges i.MX6DQ Datasheet, so 3.3V may cause problems to processor.

http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply