ERR050101: USB Endpoint conflict fixed in the A1 revision?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ERR050101: USB Endpoint conflict fixed in the A1 revision?

376 Views
atomayko
Contributor I

Hi, can anyone please confirm if "ERR050101: USB: Endpoint conflict issue in device mode" from the silicon errata of a number of the i.MXRT processors (I'm specifically interested in the i.MXRT1020) has been fixed in the A1 revision (part numbers in ending in "B")?

I'm considering using this family to develop a product that includes a USB audio interface feature, so I will need to use isochronous IN endpoints which are affected by this issue.

My 1020 EVK board has a revision A0 processor (part number ends in "A") and definitely exhibits the problem if I debug the USB audio example code and connect the device port through a hub with other devices - audio playback will stop either immediately or for no discernible reason within 5-10 minutes.

Thanks!
-Arvid

0 Kudos
Reply
1 Reply

356 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @atomayko ,

  Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.

   I have checked the errata:

https://www.nxp.com/docs/en/errata/IMXRT1020CE.pdf

kerryzhou_0-1699944831736.png

It is fixed in the A1(B) version.

Yes, you are right, the EVK is using A1 version, but you can apply the B version sample chip, then replace the on board A1 version.

 

Wish it helps you!

If you still have quesitons about it, please kindly let me know.

Best Regards,

Kerry

 

0 Kudos
Reply