Hi,
I am using Vivante gpu on customised imx6 solo board. I use sample source from this link: i.MX6DQP/DQ/DL/SL/SX GPU Demo Framework SDK, but It doesn't work. I use fb back-end (libVIVANTE-fb.so). Linux version is 3.0.35-2508-g54750ff-svn2569.
Strace on gpu_sdk_v1.00/Samples/GLES2.0/01_SimpleTriangle gives following output for example:
open("/dev/galcore", O_RDWR) = 3
ioctl(3, _IOC(0, 0x75, 0x30, 0x00), 0x7eacdc88) = -1 ENOTTY (Inappropriate ioctl for device)
ioctl(3, _IOC(0, 0x75, 0x30, 0x00), 0x7eacdc60) = -1 ENOTTY (Inappropriate ioctl for device)
However, the same program works well with SABRE board.
I have the following questions.
- Why does not customised imx6 solo board work well? I compared the customised imx6 solo board config with SABRE board config, but I did not know why it doesn't work. Atattched solo board config(solo_config) and SABRE board config(SABRE_config).
- I want to know the way and the config to work well.
Thank you,
Original Attachment has been moved to: solo_config.zip
Original Attachment has been moved to: SABRE_config.zip
解決済! 解決策の投稿を見る。
Hi, igorpadykov
01_SimpleTriangle works when /dev is writable.
Thank you.
Hi, igorpadykov
Thank you for giving me information.
I changed Kernel Configuration as follows.
Kernel Configuration
System Type
Freescale MXC Implementations
Support i.MX 6Quad Armadillo2 platform -> no check
Support i.MX 6SoloLite Armadillo2 platform -> no check
Support i.MX 6SoloLite EVK platform -> no check
Support i.MX 6Quad SABRE Lite platform -> no check
Support i.MX 6Quad SABRESD platfor -> no check
Support i.MX 6Quad SABRE Auto platform -> no check
Support i.MX 6Quad HDMIDONGLE platform -> no check
There are make errors as follows.
arch/arm/mach-mx6/usb_h2.c: In function 'hsic_start':
arch/arm/mach-mx6/usb_h2.c:185:278: error: 'PAD_CTL_DSE_40ohm' undeclared (first use in this function)
arch/arm/mach-mx6/usb_h2.c:185:278: note: each undeclared identifier is reported only once for each function it appears in
arch/arm/plat-mxc/devices/platform-imx-dma.c: In function 'imxXX_add_imx_dma':
arch/arm/plat-mxc/devices/platform-imx-dma.c:265:2: error: 'imx6q_imx_sdma_data' undeclared (first use in this function)
arch/arm/plat-mxc/devices/platform-imx-dma.c:265:2: note: each undeclared identifier is reported only once for each function it appears in
arch/arm/plat-mxc/devices/platform-imx-dma.c:268:8: error: 'addr_imx6q_to1' undeclared (first use in this function)
I did not know why make errors occur.
Please show me the solo config.
Hi toshinariagata
solo_config file has record : CONFIG_ARCH_MX6Q=y
which is not correct, as i.MX6Q and Solo are different processors
with different gpus, so there is message "Inappropriate ioctl for device".
Please refer to attached file and AN4397 Common Hardware Design for
i.MX 6Dual/6Quad and i.MX 6Solo/6DualLite
http://cache.nxp.com/files/32bit/doc/app_note/AN4397.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------