Dual display with X11 and Qt on iMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dual display with X11 and Qt on iMX6

1,543件の閲覧回数
anegoiko
Contributor III

Hi,

I'm really new in Linux and Yocto, but I'm working with a quad core iMX6 device right now. This device has 2 displays: LVDS and HDMI. I know that the QMX6 supports a dual display of LVDS and HDMI,  but I am not able to make it work. I need to run two different Qt applications in X11 environment. I'm able to run a Qt aplication (with X11) in one of the displays, but I can not run two applications simultaneously.

I have been searching, and all that I have found was related to Qt+EGLFS, but not Qt+X11. Is there any posibility to run two Qt aplication in different displays in X11?

Thanks in advance,

ラベル(4)
0 件の賞賛
返信
1 返信

836件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi anegoiko

in general dual lcd is supported in linux, please refer to attached

Linux Guide sect.4.7 Running Linux OS on the target.

I am not aware of configs to making this with Qt, seems it could be used

as starting point. i.MX6 BSPs located on

i.MX 6 Series Software and Development Tool|NXP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信