Doubts about iMX6 dual/solo design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Doubts about iMX6 dual/solo design

1,465 Views
rubenbarriuso
Contributor II

Hi community,

It the first time that I have to design a PCB based in iMX6.

I am following the design of "SABRE-AI DualLite CPU" card and "MCIMX6DL smart device platform".

My doubts are:

1 - iMX6 control ONOFF pin: I want that the device turns on itself when the I plug the power. I do not sure how this pin have to be connected. In "SABRE-AI DualLite CPU" is NC (only has a test point), so I suppose that this pin have to be NC.

2 - USB OTG on HOST mode: I have read that I can get this goal connecting USB_OTG_ID to ground. My issue is the datasheet does not define any USB_OTG_ID pin. I can see in SABRE design that this pin is connected to ENET_RX_ER,

3 - I do not sure if I have to use ENET_RX_ER pin for Ethernet 10/100 (LAN8720A). In some desigh use, and some not.

Thank you for your help

Ruben

Tags (3)
6 Replies

1,115 Views
SergioSolis
NXP Employee
NXP Employee

gusarambula  can you share some knowledge on this?

0 Kudos
Reply

1,115 Views
rubenbarriuso
Contributor II

1 - ONOFF (pin D12): reference manual says that this button input is used to request main SoC power state changes from the PMU. The "SABRE-AI DualLite CPU" design does not have this button while "MCIMX6DL smart device platform" has it. What is the different between to have and not to have this button?

2 and 3 doubt: I have solved these doubts

Ruben

1,115 Views
gusarambula
NXP TechSupport
NXP TechSupport

The ONOFF (D12) pin may be left unconnected if not used, as is the case of the i.MX6 SABRE-AI DL CPU where the power-on is controlled by the PMIC.

The SABRE SDP does have a button connected but it still uses an “auto on” feature so the board is automatically powered on when powered.

You may find more information on this in Table 2-8 of the i.MX6 Hardware Development Guide (link below).

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

1,115 Views
saurabh206
Senior Contributor III

Hi,

Send your post to imx community (e.g. i.MX Community ) to get it visible for active members.

Saurabh

0 Kudos
Reply

1,115 Views
rubenbarriuso
Contributor II

Hi,

how can I send my post to imx community?

Ruben

0 Kudos
Reply

1,115 Views
saurabh206
Senior Contributor III
0 Kudos
Reply