I am perfoming swupdate for IMX8ULP-EVK9
For that,
I taken : https://github.com/sbabic/swupdate repo and integrated in our code and I generated .swu file with sw-description and one script that I am attaching here for reference.
With this I am able to perform swupdate successfully and I can change rootfs.ext4 in partition /dev/mmcblk0p2 that you can see in sw-description file.
Now I want to perform swupdate with dualcopy for that what steps/changes I need to do in the above process?
Thanks in Advance.
Thanks @AldoG for response
The document you given I already refered that and in that there is not any explainiation specific to IMX8ULP-EVK9
Like in which partition I need to update copy of image? what needs to be exactly in sw-description file and all ,
I am providing my current partition structure for reference, But I am not able to get that which partiton I need to use to perform dualcopy swupdate?
root@imx8ulp-9x9-lpddr4-evk:~# lsblk
NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINTS
mtdblock0 31:0 0 64M 0 disk
mmcblk0 179:0 0 29.1G 0 disk
|-mmcblk0p1 179:1 0 83.2M 0 part
-mmcblk0p2 179:2 0 318.8M 0 part /
mmcblk0boot0 179:32 0 4M 1 disk
mmcblk0boot1 179:64 0 4M 1 disk
Hello,
Please refer to the following App Note:
https://docs.nxp.com/bundle/AN13872/page/topics/introduction.html
Best regards/Saludos,
Aldo.