All,
I'm using the imx6q board to do some OpenCL programmings.
Now there are two platforms of OpenCL existing on the board, one provided by FreeScale for the Vivante GPU, and the POCL(Portable OpenCL, http://pocl.sourceforge.net) for the ARMv7 CPU. It seems that, to run a program which can use both platforms, they both need to support the ICD loader (Installable Client Driver).
So I wonder whether the Vivante OpenCL support the ICD, which I didn't figure out. If not, is there any other ways allowing me to use both platforms in a program?
Hope you guys could tell me some solution.:smileyhappy:
Yabin
解決済! 解決策の投稿を見る。
Hi Zheng,
I checked with our R&D team and unfortunately we don´t support ICD loader, in this case, you just can use one platform at once. And there is no plan to start supporting it.
regards,
Andre
Hi Zheng,
I checked with our R&D team and unfortunately we don´t support ICD loader, in this case, you just can use one platform at once. And there is no plan to start supporting it.
regards,
Andre
I´m didn´t find any ICD loader in our OpenCL driver, I´m going to investigate a bit more to see if we do have it and if it is supported by our platform.
Hi,
I'm kind of in a hurry trying to find a solution to this problem.
I'm now using the open-source OCL-ICD loader. The POCL for the ARM cpu could work with it, but the vivante OpenCL still not work. I don't know whether there are other thing to do besides put an .icd file including the path of libOpenCL.so in to the /etc/OpenCL/vendors directory.
I will be really appreciate if you could help with this.