Does the dual screen display based on the IMX8MQ chip support dual interface display of QT software?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the dual screen display based on the IMX8MQ chip support dual interface display of QT software?

438 Views
ximenbingmeng
Contributor III

Hello,

we can see from the reference manual that the block diagram for achieving "dual screen display" is as follows,

ximenbingmeng_0-1718594126943.png


And I saw the following explanation,

ximenbingmeng_1-1718594172123.png

 


So if QT is in a "flow" mode, wouldn't displaying two QT interfaces work? If feasible, are there any reference examples? The kernel version we are using is 5.10.72.
Looking forward to your reply, thank you very much!

Tags (1)
0 Kudos
Reply
3 Replies

412 Views
gary_bisson
Senior Contributor III

Hi,

As far as I know it isn't possible as the i.MX 8MQ exposes 2 different DRM/KMS devices for each output, 1DCSS & 1LCDIF.

All Qt examples show multiple displays examples using 1 and only 1 DRM device:

https://doc.qt.io/qt-6/embedded-linux.html#active-outputs-and-qscreen-instances

That would work on the i.MX 8MP as it exposes 1 DRM/KMS device with several connectors/outputs (HDMI, LVDS, MIPI-DSI).

Regards

404 Views
ximenbingmeng
Contributor III

Can IMX8MQ's DCSS connect multiple outputs? For example, connecting HDMI and MIPI-DSI? Can this achieve multi screen display?

Tags (1)
0 Kudos
Reply

371 Views
gary_bisson
Senior Contributor III

No the DCSS can only connect to 1 output at a time.

0 Kudos
Reply