Hi,
I have IP-camera that output h264 stream connected to IMX8 quad max
And I'm doing a computer vision but I found out that Gstreamer's plugin 'imxvideoconvert' can't convert videostream to 3-Byte format (acceptable by neural nets).
Currently I can recieve RGBA and convert it to RGB. If I do it myself in code it will spend up to 100% of CPU core time. It leaves no space for other computations.
`gst-inspect-1.0 -a |grep imxvideoconvert` shows that outputs colors may be 2-byte or 4-byte only.
I've briefly read https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf but I could find any relative info there. Moreover it uses $video_decoder_plugin that's not declared anywhere.
What is fastest way to get raw video in BGR/RGB format?
Thanks
Hello korabelnikov,
One can test with nxp version of gstreamer plugins : imx-gst1.0-plugin using
sect.7.3.15 Video conversion on the Linux Guide.
Make sure that you are working with the latest BSP.
it can be posted on gstreamer-imx github page :
https://github.com/Freescale/gstreamer-imx/issues
Regards
Thank you for a fast response,
I just checked first tip, went to linux use guide
7.3.15 Video conversion
There are three video conversion plugins, imxvideoconvert_ipu, imxvideoconvert_g2d, and imxvideoconvert_pxp
first two absent in my gstreamer, third doesn't support 3byte formats
I just started build 5.4.47 instead of 5.4.24. Does new build may help?
Also i've created issue on the github