Does imx8mp boot rom support serial download via USB 1.1 12 Mbps

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does imx8mp boot rom support serial download via USB 1.1 12 Mbps

519 次查看
jaylbrown
Contributor II

We are bringing up a new board with the iMX8MP.

We can load and run flash.bin via uuu over USB port 2 using USB high speed 480 Mbps.

We have USB port 1 connected through a TI USB port isolator "ISO USB 111" which only passes USB low speed or USB full speed 12Mbps. uuu fails after 1% to 3% shown and ends with LIBUSB_ERROR_PIPE.

Using a scope, the signals at the iMX8MP side of the isolator look very clean.

Does the iMX8MP boot rom support USB full speed over the serial download protocol?  

Thanks.

0 项奖励
回复
1 回复

501 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

For serial download recommend you to use the USB1 , do not use usb2 port.

 

0 项奖励
回复