Does imx-android-l5.1.1_2.1.0-ga support DRM?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does imx-android-l5.1.1_2.1.0-ga support DRM?

1,444件の閲覧回数
calvinyu
Contributor II

Hi

We have a project which uses iMx6 Quad and Android 5.1.

The BSP version is imx-android-l5.1.1_2.1.0-ga.

There are 2 questions.

1. Does the imx-android-l5.1.1_2.1.0-ga BSP support DRM feature?

2. How to write the DRM key to the device ?The DRM key is from google.

B.R

Calvin

0 件の賞賛
返信
3 返答(返信)

990件の閲覧回数
pratik0403
Contributor I

Hi,

 

I have couple of questions with the same Widevine compliance on Android.

1. Is "Widevine level 1 compliance for DRM" implemented/available for IMX6 on Android platform? or Do we need to purchase separately?

2. If it is already implemented, then where we can find it's relevant document?

 

Thanks & Regards,

Pratik

0 件の賞賛
返信

990件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Calvin

it is supported as separate patch (not included in default

Android release), note customer needs license with google,

please contact local marketing for that.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

990件の閲覧回数
calvinyu
Contributor II

Hi igor

Thank you for your information.

0 件の賞賛
返信