Does iMX7D support LPDDR2-800MHz and LPDDR3-933MHz?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does iMX7D support LPDDR2-800MHz and LPDDR3-933MHz?

Jump to solution
810 Views
simonlu
Contributor I

Hi,

I am trying to implement two kinds of the RAM - LPDDR2-800Mhz and LPDDR3-933Mhz, as I know, the iMX7D can support up to 1066Mhz for both LPDDR2 and LPDDR3, but cloud it downgrade to the 800Mhz for LPDDR2, or 933Mhz for LPDDR3? Please advise, thank you!

Labels (1)
0 Kudos
Reply
1 Solution
660 Views
igorpadykov
NXP Employee
NXP Employee

Hi Simon

yes these lower grades are also supported.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
661 Views
igorpadykov
NXP Employee
NXP Employee

Hi Simon

yes these lower grades are also supported.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------