Does iMX7D support LPDDR2-800MHz and LPDDR3-933MHz?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does iMX7D support LPDDR2-800MHz and LPDDR3-933MHz?

跳至解决方案
808 次查看
simonlu
Contributor I

Hi,

I am trying to implement two kinds of the RAM - LPDDR2-800Mhz and LPDDR3-933Mhz, as I know, the iMX7D can support up to 1066Mhz for both LPDDR2 and LPDDR3, but cloud it downgrade to the 800Mhz for LPDDR2, or 933Mhz for LPDDR3? Please advise, thank you!

标签 (1)
0 项奖励
回复
1 解答
658 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Simon

yes these lower grades are also supported.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
659 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Simon

yes these lower grades are also supported.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------