Does i.MX8M mini USBx_VBUS pin can directly connect to the 1.8 V or 3.3V?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does i.MX8M mini USBx_VBUS pin can directly connect to the 1.8 V or 3.3V?

957 次查看
Danube
Contributor IV

Does i.MX8M mini USBx_VBUS pin can directly connect to the 1.8 V or 3.3V?

WE know add 30k ohm when connect to 5V.

0 项奖励
回复
1 回复

888 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  From hardware specs of the i.MX8Mm [Table 9 (Operating ranges) in IMX8MMCEC],

USB1_VBUS and USB2_VBUS should be in range 0.800 -- 3.60 V, typ = 1.40 V.

  So it is possible to connect the VBUS to any output of allowed voltage, but

it is USB VBUS input detect signal, which reflects USB VBUS, used in USB protocols.  

https://www.nxp.com/docs/en/data-sheet/IMX8MMCEC.pdf 

Regards,

Yuri.

0 项奖励
回复