Does i.MX6 Dual Lite support dual LVDS display output?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does i.MX6 Dual Lite support dual LVDS display output?

ソリューションへジャンプ
1,275件の閲覧回数
m_c
Senior Contributor I

Does i.MX6 Dual Lite support dual LVDS display output in same content or different content?

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
747件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

yes, it supports: from sect.40.4.1 Input Parallel Display Ports IMX6SDLRM  :

One or Two (DI0, DI1) parallel RGB input ports are supported (configurable)...

sect.40.4.2 Output LVDS Ports:

There are 2 LVDS channels. These outputs are used to communicate RGB data and

controls to external LCD displays.

• Separate 2 channel output (2 input sources from IPU).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
748件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

yes, it supports: from sect.40.4.1 Input Parallel Display Ports IMX6SDLRM  :

One or Two (DI0, DI1) parallel RGB input ports are supported (configurable)...

sect.40.4.2 Output LVDS Ports:

There are 2 LVDS channels. These outputs are used to communicate RGB data and

controls to external LCD displays.

• Separate 2 channel output (2 input sources from IPU).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信