Does i.MX6 Dual Lite support dual LVDS display output?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does i.MX6 Dual Lite support dual LVDS display output?

Jump to solution
1,484 Views
m_c
Senior Contributor I

Does i.MX6 Dual Lite support dual LVDS display output in same content or different content?

Labels (2)
Tags (2)
0 Kudos
Reply
1 Solution
956 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

yes, it supports: from sect.40.4.1 Input Parallel Display Ports IMX6SDLRM  :

One or Two (DI0, DI1) parallel RGB input ports are supported (configurable)...

sect.40.4.2 Output LVDS Ports:

There are 2 LVDS channels. These outputs are used to communicate RGB data and

controls to external LCD displays.

• Separate 2 channel output (2 input sources from IPU).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
957 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

yes, it supports: from sect.40.4.1 Input Parallel Display Ports IMX6SDLRM  :

One or Two (DI0, DI1) parallel RGB input ports are supported (configurable)...

sect.40.4.2 Output LVDS Ports:

There are 2 LVDS channels. These outputs are used to communicate RGB data and

controls to external LCD displays.

• Separate 2 channel output (2 input sources from IPU).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply