Does i.MX 6UltraLite Processor Product Support Ethernet?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does i.MX 6UltraLite Processor Product Support Ethernet?

387 次查看
klinsmann_mah5
Contributor I

As my requirement required to get a MCU/CPU which supports dual CAN, dual Ethernet and at least 2 USB, I chance about i.MX 6UltraLite Processor. However, the product does not have the Ethernet column for which the data sheet states that there is 2.

May I ask if the microchips consist of Ethernet?

Also, is there any other recommendation of MCU/MPU my requirement stated?

0 项奖励
2 回复数

326 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

About the MCU, I have confirmed it with my colleague some of the RT1060 can support your need dual CAN, dual Ethernet and at least 2 USB.

MIMXRT1062CVL5A
MIMXRT1061CVL5A
MIMXRT1062DVL6A
MIMXRT1061DVL6A
MIMXRT1062CVJ5A
MIMXRT1061CVJ5A
MIMXRT1062DVJ6A
MIMXRT1064CVL5A
MIMXRT1064DVL6A

Hope this can do help for you.

Have a nice day

Rita

0 项奖励

326 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

The i.MX6UL can support the Ethernet , and support 2Ethernet. Details you can see the datasheet. Here the i.MX7D also can support your need.i.MX 7Dual Applications Processors | Dual Arm® Cortex®-A7 + Cortex-M4 | NXP
Have a great day,
Rita

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励