Does g2d support G2D_RGB888 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does g2d support G2D_RGB888 ?

1,294件の閲覧回数
brenhale
Contributor I

The G2D API format enumeration describes G2D_RGB888 as a 24-bit RGB option (enum #10).

However attempts to use this, even for very simple blit operation yield errors for either invalid src or dst format.

g2d_blit_2d: Invalid src format 10!

There is no errata for lack of support for this. Should it work?

Tested on imx8mm.

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,174件の閲覧回数
michaelnazzaren
Contributor I

Hi

I have the same problem. Can we have a folowup? Android 10 is my bsp base on

int ret;
void* g2dHandle = getHandle();
struct g2d_buf s_buf, d_buf;
struct g2d_surface s_surface, d_surface;

s_buf.buf_paddr = tmpBuf.mPhyAddr;
s_buf.buf_vaddr = tmpBuf.mVirtAddr;
d_buf.buf_paddr = dstBuf.mPhyAddr;
d_buf.buf_vaddr = dstBuf.mVirtAddr;

s_surface.format = G2D_RGB888;
s_surface.planes[0] = (long)s_buf.buf_paddr;
s_surface.left = 0;
s_surface.top = 0;
s_surface.right = src->width();
s_surface.bottom = src->height();
s_surface.stride = src->width();
s_surface.width = src->width();
s_surface.height = src->height();
s_surface.rot = G2D_ROTATION_0;

d_surface.format = (g2d_format)convertPixelFormatToG2DFormat(dst->format());
d_surface.planes[0] = (long)d_buf.buf_paddr;
d_surface.planes[1] = (long)d_buf.buf_paddr + dst->width() * dst->height();
d_surface.left = 0;
d_surface.top = 0;
d_surface.right = dst->width();
d_surface.bottom = dst->height();
d_surface.stride = dst->width();
d_surface.width = dst->width();
d_surface.height = dst->height();
d_surface.rot = G2D_ROTATION_0;

ret = mBlitEngine(g2dHandle, (void*)&s_surface, (void*)&d_surface);
if (ret == 0) {
mFinishEngine(g2dHandle);
}

0 件の賞賛
返信

883件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

confirmed that imx8mm doesn't support this, only imx8qxp and imx8qm support this format

0 件の賞賛
返信

1,227件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

refer to the gpu api, gpu should support this format, but what's your case? did you capture video as rgb888 from camera?

0 件の賞賛
返信