Does WDT keep running after kernel crash?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does WDT keep running after kernel crash?

652件の閲覧回数
viniciusmaciel
Contributor II

Hi,

I want to know if the Watchdog timer continue to run even after the linux kernel crash?

In my current system, Linux 4.9.11 on wandboard, after the linux kernel crashes nothing happen and  I have to reboot manually, which will not be possible when my system goes to field.

ラベル(3)
タグ(2)
0 件の賞賛
1 返信

511件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vinicius

in general it should work except cases, when accidentally

wdt clock sources were disabled, described in sect.70.3 Clocks

Chapter 70 Watchdog Timer (WDOG) i.MX6SDL Reference
Manual or changed bits WDZST, WDBG, register WDOGx_WCR.
http://www.nxp.com/assets/documents/data/en/reference-manuals/IMX6SDLRM.pdf 


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛