Hello,
I want to run openAMP on iMX6sx-sdb. ARM A9 core runs Linux and M4 core runs vxWorks.
The communication between A9 and M4 uses openAMP framework.
Does Freescale iMX6 Linux BSP (Yocto project) support openAMP?
Thanks,
Miles
Hi Miles
yes it is supported, description can be found in attached Linux Manual
Chapter 53.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
I read the attached Linux Manual Chapter 53 and knew that Freescale’s solution to the multi-core architecture with different OSs is a multi-core communication (MCC) protocol. MCC is different from openAMP.
The key components and capabilities provided by the OpenAMP Framework include remoteproc and RPMsg.
So Freescale Linux doesn't support openAMP. Right?
Best regards,
Miles