Hello everyone,
i'm not able to find the right documentation for my type of board (png: picOfCon).
On
http://www.nxp.com/products/single-chip-modules/quick-start-board-for-scm-i.mx-6dq:QWKS-SCM-IMX6DQ
it is exactly my board illustrated. However the docu
http://www.nxp.com/products/single-chip-modules/quick-start-board-for-scm-i.mx-6dq:QWKS SCM-IMX6DQ?tab=Design_Tools_Tab
seems to refer to a version of the board with a different connector in that area where my flat cable connector is (png: wrong board).
On page 12 of the schematic pdf "SPF-28927-D" there is the pin configuration explained. But not for my kind of flat cable connector with 15 pins. On my board is a sticker with the following information "700-28927 REV X2 , SCH-28927 REV B3 , 04/14/16 35960-0093" if it helps. I would like to get the documentation of this board version (or just this connector).
Best regards
Patrick
Seems to be the MIPI 15 Pin CSIx camera interface?!
May somebody confirm that with a source.
Hi Patrick,
Could you tell me if you want to use the connector to realize some functions or something else?
Have a nice day
Rita
Hi,
that's exactly the place where the wrong (other board version) documentation can be found.
Hi Patrick,
I will do further confirming for you. And then give you reply.
Have a nice day
Rita
Hi Patrick,
You can get all the infomations about the your board here http://www.nxp.com/products/single-chip-modules/quick-start-board-for-scm-i.mx-6dq:QWKS-SCM-IMX6DQ . Here if you mainly need the infromantions on the flat cable connector?
Have a great day,
Rita
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------