Do the timers in i.MX6ULL can support quadrature (incremental) encoder input ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Do the timers in i.MX6ULL can support quadrature (incremental) encoder input ?

1,949件の閲覧回数
jimmyli
Contributor IV

Hi,

     We are evaluting the i.MX6ULL for our project.

     In the project, we need to encode one magnetic encoder quadrature input (A/B), and one signal output.

     We find i.MX6ULL has not QDC, so we consider that if the timer in i.mx6ull can support this function?

     Hope you can help to check with us.

     Thanks very much.

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,898件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

There is no QDC in i.MX6ULL. So the feature is not supported.

0 件の賞賛
返信

1,896件の閲覧回数
jimmyli
Contributor IV

Hi Jimmychan,

      Get it. Thanks.

      Yes, i.MX6ULL hasn't QDC, so I conside that whether the quadrature encoder inputs can be captured by GPT capture function, but I still can't be sured about it.

      Do you have some tips for this ?

      Thanks.

jimmyli_0-1712481873545.png

----i.MX6ULL GPT capture function

 

0 件の賞賛
返信

1,877件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

I searched around internal database and cannot find any example code about this.

0 件の賞賛
返信

1,850件の閲覧回数
jimmyli
Contributor IV

Hi Jimmychan,

       Get it.

       Thanks very much.

0 件の賞賛
返信