Do the timers in i.MX6ULL can support quadrature (incremental) encoder input ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Do the timers in i.MX6ULL can support quadrature (incremental) encoder input ?

563 次查看
jimmyli
Contributor IV

Hi,

     We are evaluting the i.MX6ULL for our project.

     In the project, we need to encode one magnetic encoder quadrature input (A/B), and one signal output.

     We find i.MX6ULL has not QDC, so we consider that if the timer in i.mx6ull can support this function?

     Hope you can help to check with us.

     Thanks very much.

标签 (1)
0 项奖励
回复
4 回复数

512 次查看
jimmychan
NXP TechSupport
NXP TechSupport

There is no QDC in i.MX6ULL. So the feature is not supported.

0 项奖励
回复

510 次查看
jimmyli
Contributor IV

Hi Jimmychan,

      Get it. Thanks.

      Yes, i.MX6ULL hasn't QDC, so I conside that whether the quadrature encoder inputs can be captured by GPT capture function, but I still can't be sured about it.

      Do you have some tips for this ?

      Thanks.

jimmyli_0-1712481873545.png

----i.MX6ULL GPT capture function

 

0 项奖励
回复

491 次查看
jimmychan
NXP TechSupport
NXP TechSupport

I searched around internal database and cannot find any example code about this.

0 项奖励
回复

464 次查看
jimmyli
Contributor IV

Hi Jimmychan,

       Get it.

       Thanks very much.

0 项奖励
回复