Distro with NO GPU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Distro with NO GPU

889 次查看
razriel
Contributor II

I am currently using imx8mn-ddr4-evk with with fsl-imx-xwayland distro and imx-image-core.

My Target board application processor will have 1 core only with no GPU,no screen, no touchscreen, no audio in nor audio out.

I have updated the kernel device tree accordingly. 

I have noticed the ditro still have the following services running:

psplash-basic
psplash-network
psplash-quit
psplash-systemd
weston

what is the way to modify the distro so it wont install these elements to the distro ?

is there any pros of having as part of the distro ?

Thanks

Roy

 

标签 (1)
0 项奖励
回复
2 回复数

883 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You need weston if you are going to use Wayland, the ps* can be eliminated if you are not going to use LCD, eliminated from Kernel and device tree.

 

Regards

0 项奖励
回复

872 次查看
razriel
Contributor II

I do not intend to use wayland my question is how do I eliminate parts of the distro without breaking stuff.

0 项奖励
回复