Dear Sir or Madam,
Hello.
I have question about freescale's recommendation about distance of DDR3 signal lines in i.MX6.
Refer to "Table 3-1. Stackup implementation" in Hardware Development Guide for i.MX6DQ6SDL, Rev. 1.
Trace width is 4.7[Mils] with Single ended.
Generally, distance of DDR3 signal lines are recommended twice of length of the Trace width.
But, the distance of signal lines of SABRE-AI were about 4.0 [Mils].
It is very narrow.
[Question]
Could you tell me the recommendation about distance of signal lines?
Or, please give me your advice.
Best Regards,
Keita
已解决! 转到解答。
The restriction of DDR3 signal traces spacing of 2x of traces width is important on a long (longer than approx 3.5 inches) DDR3 buses that cause a high signal crosstalk between adjacent traces. In case of relatively short DDR3 bus (1 - 2 inch), as on the i.MX6 SABRE SD or i.MX6 SABRE AI boards, this restriction is much less significant and may not be followed. So, the DDR3 signal traces spacing of 4 - 5 mils is pretty acceptable in that case.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
The restriction of DDR3 signal traces spacing of 2x of traces width is important on a long (longer than approx 3.5 inches) DDR3 buses that cause a high signal crosstalk between adjacent traces. In case of relatively short DDR3 bus (1 - 2 inch), as on the i.MX6 SABRE SD or i.MX6 SABRE AI boards, this restriction is much less significant and may not be followed. So, the DDR3 signal traces spacing of 4 - 5 mils is pretty acceptable in that case.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------