Hi all,
I'd like to display a video (or the camera) in a small window over Chrome. We need to achieve this on two systems: the imx6dl and imx8mm.
I tried this simple pipeline but the video is flickering (maybe because chrome and gstreamer are both writing on the same fb).
gst-launch-1.0 filesrc location=Spin_1.mp4 typefind=true ! qtdemux ! queue ! vpudec ! imxg2dvideosink window-x-coord=0 window-y-coord=0 window-width=640 window-height=360
Any idea? Playing the media with chrome is out of question because of missing hw acceleration.
Thanks
Paolo Gentili
已解决! 转到解答。
Hello pgentili,
Which bsp are you using? which distro? because I used the 5.4.47 and it works like a charm.
Regards
Hi, I'm using yocto krogoth on the iMX6DL and yocto zeus on iMX8MM.
The first test I did was only performed on the imx6dl and it's indeed flickering. On the imx8mm I tried only after your suggestion and it's working fine (with differente sink: waylandsink).
Since on the imx6 we already have implemented a different solution based on the second frame buffer we can close this topic.
Thanks.