Display pixel clock limitation to 74.25 MHz

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Display pixel clock limitation to 74.25 MHz

12,228 Views
sebastian1
Contributor II

Hi,

I'm using a board with the IMX8 SoC and 4.14.98 IMX kernel.

I'm trying to add support for a MIPI-DSI display (800x480@60Hz) that needs a pixel clock of ~25MHz.

The problem is that there is a minimum limit for the pixel clock of 74.25MHz, both in the LCDIF and DCSS driver.

In the drivers there is mentioned a TODO about fixing this minimum limit.

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/gpu/drm/mxsfb/mxsfb_drv.c?h=imx_4....
https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/gpu/imx/dcss/dcss-dtg.c?h=imx_4.14...

Any plans or timeline on fixing this clock limit?

Thank you!

Labels (1)
23 Replies

1,648 Views
sebastian1
Contributor II

Hi Santiago,

Could you please show me the patch you worked to allow dsi_lanes = 1?

Thank you!

0 Kudos
Reply

560 Views
sotero
Contributor III

Hi Sebastian. For enabling support for 1 lane you have to patch drivers/gpu/drm/bridge/nwl-dsi.c:

@@ -664,7 +655,7 @@ static bool nwl_dsi_bridge_mode_fixup(struct drm_bridge *bridge,
 
        DRM_DEV_DEBUG_DRIVER(dsi->dev, "lanes=%u, data_rate=%lu\n",
                             config->lanes, config->bitclock);
-       if (config->lanes < 2 || config->lanes > 4)
+       if (config->lanes < 1 || config->lanes > 4)
                return false;

Maybe the lines numbers are not the same in your linux kernel sources. At this moment I'm using linux-imx_4.19.35_1.1.0. This experimental kernel version from NXP already has all the patches about the pixelclock limitations.

0 Kudos
Reply

560 Views
sebastian1
Contributor II

Hi Santiago,

I was doing this obvious modification as well, but I was under the impression that it doesn't work.

In fact it was working but I was measuring the wrong signal.

Thank you for your help!

0 Kudos
Reply