Dispaly is not working in IMX6Q based custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dispaly is not working in IMX6Q based custom board

1,181 Views
ashokp
Contributor I

Hi All,

I am using IMX6Q based custom board. I am trying to port the Android Kitkat downloaded from free-scale website for sabreSD board. The The hdmi display is not working. I observed the device node for frame buffer is not created. I attached console log and my config file for more details

Thanks,
P.Ashok

Original Attachment has been moved to: IMX6Q_boot_log.txt.zip

Original Attachment has been moved to: config.txt.zip

Labels (3)
Tags (1)
0 Kudos
Reply
1 Reply

603 Views
Yuri
NXP Employee
NXP Employee

HDMI interface should not be used with HDMI-to-DVI converter.

Please try using "true" HDMI monitor / TV.

As mentioned in the next thread,

"iMX6Q: HDMI not working"

https://community.freescale.com/message/393635#393635

one may try to adapt the following solution :

http://boundarydevices.com/dvi-support-on-i-mx6-boards/


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply