Dirty COW

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
860件の閲覧回数
andreyreyes
Contributor II

Hi i.MX Community,

I noticed there was a BSP/Linux release from NXP on 2016-10-10, "L4.1.15_2.0.0", but the kernel fix for Dirty COW was committed on 2016-10-18.

I just started working on an SABRE board (IMX6Q-SDB) and I am new to NXP, board bring-up and Yocto. With that said, these are my questions:

  • Does NXP provide security updates?
  • I kind of have the feeling this is something I am going to have to patch myself somehow in Yocto but my searches haven't return anything meaningful on fixing dirty COW in Yocto.
    • Any guidance on this?
    • Would it work if I just patch the kernel like they did here?

Thanks,

-Andrey Reyes-

ラベル(3)
0 件の賞賛
1 解決策
427件の閲覧回数
art
NXP Employee
NXP Employee

Q. Does NXP provide security updates?

A. No, we do not provide the general kernel-related security updates by ourselves.

Q. Would it work if I just patch the kernel like they did here?

A. I think Yes.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
1 返信
428件の閲覧回数
art
NXP Employee
NXP Employee

Q. Does NXP provide security updates?

A. No, we do not provide the general kernel-related security updates by ourselves.

Q. Would it work if I just patch the kernel like they did here?

A. I think Yes.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛