Hi,
I was surprised this BSP( L3.14.52 ) didn't support DirectFB anymore but I prefer this backend.
So I tried to build it then following ERROR occurred.
$ cd fsl-release-bsp
$ repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.52-1.1.0_ga
$ repo sync
$ source setup-environment
#### command #1
$ DISTRO=fsl-imx-dfb MACHINE=imx6qpsabreauto source fsl-setup-release.sh -b build-dfb
#### command #2
#### $ MACHINE=imx6qpsabresd source fsl-setup-release.sh -b build-dfb -e dfb
#### error log
$ bitbake fsl-image-qt5
ERROR: OE-core's config sanity checker detected a potential misconfiguration.
Either fix the cause of this error or at your own risk disable the checker (see sanity.conf).
Following is the list of potential problems / advisories:
DISTRO 'fsl-imx-dfb' not found. Please set a valid DISTRO in your local.conf
Summary: There was 1 ERROR message shown, returning a non-zero exit code.
Does anyone already tried to build DirectFB?
How can I get fsl-imx-dfb conf?
Can anyone help me? Please let me know how to avoid this error.
Thanks.
Solved! Go to Solution.
HI torus1000
please refer to attached part of Freescale_Yocto_Project_User's_Guide.pdf
that means that it is necessary to apply to third party or contact
NXP Professional Services for developing this backend
http://www.nxp.com/pages/freescale-professional-services:PROFESSIONAL-SERVICES
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
bitbake fsl-image-qt5
NOTE: Your conf/bblayers.conf has been automatically updated.
ERROR: OE-core's config sanity checker detected a potential misconfiguration.
Either fix the cause of this error or at your own risk disable the checker (see sanity.conf).
Following is the list of potential problems / advisories:
DISTRO 'fsl-imx-fb' not found. Please set a valid DISTRO in your local.conf
is also not working is there any issue with the distro or is there any other alternative for it??
HI torus1000
please refer to attached part of Freescale_Yocto_Project_User's_Guide.pdf
that means that it is necessary to apply to third party or contact
NXP Professional Services for developing this backend
http://www.nxp.com/pages/freescale-professional-services:PROFESSIONAL-SERVICES
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Igor
Thank you for your advice. It seems not so easy.
Now I understand the ERROR suggested missing conf file. So I made <yocto>/source/meta-bsp-release/imx/meta-sdk/conf/distro/fsl-imx-dfb.conf then error was cleared.
BR