Did i.MX6Q support busybox's poweroff and halt command

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Did i.MX6Q support busybox's poweroff and halt command

847 Views
bakbad
Contributor III

Hello, NXP

When i used busybox-1.22.1's poweroff and halt command to power down the system, it did not work, but the reboot command could work well. With poweroff and halt command to turn off the system ,it has some messages like this:

The system is going down NOW!

Sent SIGTERM to all processes

Sent SIGKILL to all processes

Requesting system poweroff

reboot: System halted

But the custom board is still power on.Can somebody help me?(P.S. Linux version 3.14.52)

Best Regards,

bo xu

Labels (4)
0 Kudos
2 Replies

628 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi bo,

There´s no support officially for busybox of part of NXP, they support uboot, however you can see other cases where have running.

busybox on the i.MX6 sabre sd platform in a few commands 

https://community.nxp.com/message/930713 

Regards

0 Kudos

628 Views
bakbad
Contributor III

Hi Bio_TICFSL,

Thanks for your advice.

Best Regards

0 Kudos