i.MX8MQ EVK can not powerdown with poweroff or halt command

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8MQ EVK can not powerdown with poweroff or halt command

1,202 Views
bakbad
Contributor III

Hello, NXP

When I used poweroff or halt, reboot command in linux-4.9.88 , they can not work.And i have uploaded the log from serial. Could you give me some help with this problem。

Best Regards,

bo xu

Labels (2)
0 Kudos
Reply
2 Replies

1,030 Views
jimmychan
NXP TechSupport
NXP TechSupport

According to BSP team, this problem occurs because of an Wi-Fi issue.

You can reboot the board if you change kernel parameters.

Add "pci=nomsi"  to mmcargs in u-boot in order to fix Wi-Fi.

1,030 Views
bakbad
Contributor III

Hi jimmychan,

Thanks for your advice.

Best Regards.

0 Kudos
Reply