Device driver availability for IMXAI2ETH-BRC daughter board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Device driver availability for IMXAI2ETH-BRC daughter board

1,474 Views
krishnasrivasta
Contributor I

Hello,

We am planning to buy below NXP Sabre boards for AVB development purpose:

1. MCIMX6QAICPU2

2. IMXAI2ETH-BRC

See the link below:

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

We have some below queries, please address it.

Q. Will we get device driver for "IMXAI2ETH-BRC" daughter board along with the board BSP?

Krishna Srivastava

Senior Software Engineer

krishna.srivastava@aricent.com<mailto:krishna.srivastava@aricent.com> | Mobile +91 9686467869

<../../../../../gur39887/AppData/Local/Microsoft/Windows/Temporary%20Internet%20Files/Content.IE5/O5KCXCI1/CANM8JID>

"DISCLAIMER: This message is proprietary to Aricent and is intended solely for the use of the individual to whom it is addressed. It may contain privileged or confidential information and should not be circulated or used for any purpose other than for what it is intended. If you have received this message in error, please notify the originator immediately. If you are not the intended recipient, you are notified that you are strictly prohibited from using, copying, altering, or disclosing the contents of this message. Aricent accepts no responsibility for loss or damage arising from the use of the information transmitted by this email including damage from virus."

0 Kudos
1 Reply

1,346 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Krishna,

The following Community thread may be useful for what are you looking for:

how to config the Ethernet-AVB system with the I.MX6q SABRE-AI Platform?

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos