IMX6SDLRM.pdf contain application note regarding to procedure of EIM flash access at section 22.7.
In following case, I suppose "aah write to base address(CS0) + offset address(555h) by 16bits access".
what does mean "<<1" notation?
22.7.6.2 Spansion Flash Synchronous Mode Configuration
WR16('CS0+('h0555<<1),'h00aa);
Best Regards,
Kazuma Sasaki.
Solved! Go to Solution.
Hi Kazuma
"<<1" notation means shift left by one position. Flash devices capable of burst operations
do not power up in burst mode. The devices start out in asynchronous
mode, and then must be put into burst mode by programming the configuration register.
Spansion configuration for burst access for example is described on :
http://www.eetasia.com/STATIC/PDF/200806/EEOL_2008JUN26_STOR_EMS_AN_01.pdf?SOURCES=DOWNLOAD
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Kazuma
"<<1" notation means shift left by one position. Flash devices capable of burst operations
do not power up in burst mode. The devices start out in asynchronous
mode, and then must be put into burst mode by programming the configuration register.
Spansion configuration for burst access for example is described on :
http://www.eetasia.com/STATIC/PDF/200806/EEOL_2008JUN26_STOR_EMS_AN_01.pdf?SOURCES=DOWNLOAD
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Did you mean that "WR16('CS0+('h0555<<1),'h00aa)" equal to "WR16('CS0+('h0aaa),'h00aa)"?
Is it right?
I checked following document.
I think that we should shift left by one position such as application note when we access to the flash device by byte accessing case. If my understanding is not correct, could you elaborate more detail?
Best Regards,
Kazuma Sasaki.
Hi Kazuma
init sequence is defined by nor flash specs, suggest to contact vendor
support for this specific nor flash for more details about nor initialization sequence.
Best regards
igor
Hi Igor,
Okay, I appreciate your support.
Best Regards,
Kazuma Sasaki.