Hello:
I am trying to get the my Java app to debug over USB cable. I plug-in the USB cable from the i.MX53 SABRE tablet to my Window 7 (32-bit). I go under C:\Users\mydevuser\.android folder to modify the adb_usb.ini file by adding 0x15a2. I build a "hello world" app, but I cannot able to download to the SABRE tablet.
Can you help me to setup USB bridge to the SABRE tablet so I can develop JAVA / Eclipse application?
Mike
已解决! 转到解答。
Hi:
I got it working. In the imx-andriod-r10.4\tool\android_usb_fsl.zip is the USB driver. The i.MX Andriod customize the USB driver.
In the i.MX_Android_R10.4_User_Guide.html have one line talk about the tool\android_usb_fsl.zip that need to be install inorder for the Win7 USB driver to attach to.
"Unpack the freescale Android USB win driver in the release package tool\android_usb_fsl.zip"
Mike
a collection of steps to get adb running:
https://community.freescale.com/docs/DOC-1373
Please, let me know if you can list your device.
Hi:
I got it working. In the imx-andriod-r10.4\tool\android_usb_fsl.zip is the USB driver. The i.MX Andriod customize the USB driver.
In the i.MX_Android_R10.4_User_Guide.html have one line talk about the tool\android_usb_fsl.zip that need to be install inorder for the Win7 USB driver to attach to.
"Unpack the freescale Android USB win driver in the release package tool\android_usb_fsl.zip"
Mike
Hi Mike,
Did you try to restart the ADB server on the Windows PC after updating the adb_usb.ini file? The shell commands to do this are
adb kill-server
adb start-server
Also, did you verify that ADB is enable on your device under Setting->Applications->Development->USB Debugging?
Does the device show up in the Windows Device Manager as an "Android Phone" with correct VID and PID?
Oliver