Debian on i.mX287

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debian on i.mX287

970 Views
carloventrella
Contributor I

Hi, all.

I'm very newbie. Is it possibile to install debian within this processor?

If not, which processor supports it?

UPDATE

The board in issue is this: PLC operator panel, PLC with HMI

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

774 Views
fabio_estevam
NXP Employee
NXP Employee

Yes, it is possible.

Here is a tutorial for mx23 that you can refer to and adapt it to mx28:

https://eewiki.net/display/linuxonarm/iMX233-OLinuXino

Regards,

Fabio Estevam

0 Kudos
Reply

774 Views
carloventrella
Contributor I

Thank you Fabio.

I updated the question with the spec of the board and maybe I've too low memory to mount debian.

However, what do you mean with 'adapt it to mx28'? Should I change something?

For example in the section Bootloader -> patches I see:

wget -c https://rcn-ee.com/repos/git/u-boot-patches/v2015.10-rc3/0001-mx23_olinuxino-uEnv.txt-bootz-n-fixes.patch

patch -p1 < 0001-mx23_olinuxino-uEnv.txt-bootz-n-fixes.patch

That seems to be specific for mx23 .. isn't it?

0 Kudos
Reply

774 Views
jamesbone
NXP TechSupport
NXP TechSupport

Sure it is possible,  in fact we have an UBUNTU BSP for the i.MX28EVK that you find in the following link, and since UBUNTU it is a distro from Debian, there is no limitation on the usage of Debian with any of the i.MX

i.MX287 Processors|Dual Ethernet|Freescale

0 Kudos
Reply