De-interlace Capture Device issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

De-interlace Capture Device issue

1,143件の閲覧回数
m_c
Senior Contributor I

Add apply patch at <De-interlace Capture Device>, the image became blur. Is this right? How to improve it?

01_original = Freescale Android JB4.3 1.1.0

14132_14132.png03_original_zoom.png

02_deinterlace.png

After apply deinterlance patch

14134_14134.png04_deinterlace_zoom.png

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

786件の閲覧回数
rotechen
Contributor I

I have same issue with m.c. I using "Freescale Android JB4.3 1.1.0" with iMX6DL.

If I don't add the patch, the image will some interlacing artifacts in edge of motion object. It show as below.

CSI_MEM_side_effect.png

 

If i adding apply patch at <De-interlace Capture Device>, the image became blur. How to improve it?

0 件の賞賛
返信

786件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

That patch is rather old for JB4.3, it shouldn't be necessary

Are you able to see the images sharp without the patch? ( I see that the image you posted is at 500% zoom so i cannot determine it)

786件の閲覧回数
m_c
Senior Contributor I

Without patch

01_original.png

With patch

02_deinterlace.png

0 件の賞賛
返信