Hi Team,
We are facing an issue on DVFS in imx7dsabresd. we could able to measure the voltage in TP4 test point on board it always showing 1.296V on every frequency (729000,996000,1200000 Mhz). We have tested some BSP versions and It have been noticed that the issue is coming on the BSP version 4.14.98_2.0.0 and 4.14.78_1.0.0. The DVFS is working properly on 4.9.88-2.0.0_ga and L4.1.15_1.2.0 (image only). when we compare 4.9.88-2.0.0 and 4.14.98_2.0.0 we could able to find out that imx7-cpufreq.c ( drivers/cpufreq/imx7-cpufreq.c ) file is missing on 4.14.98_2.0.0 and some configuration changes. could you please help on this ?
imx7-cpufreq.c appears to have been replaced by the generic cpufreq-dt implementation somewhere between 4.9 and 4.14.
If you already had a working 4.9 setup, then to upgrade to 4.14 you'll likely just need to
Hello Muhammed,
Can you please share your DTS file, The voltage and frequency changes are passed to the linux kernel via the u-boot dtb file. In the dts (source file for dtb). By adding or modifying the entry in the dts file, the system can work at lower frequencies.. here is what the current dts file has:
cpu0: cpu@0 {
compatible = "arm,cortex-a7";
device_type = "cpu";
reg = <0>;
operating-points = <
/* KHz uV */
996000 1075000
792000 975000
>;
Add entries below the "792000 975000" in the dts file.