i am using DS90UB914A-Q1/913 camera to capture image
i can receive 913 camera data and save those,but the image is green. like below:
the 913 camera format is ccir601 8bit (UYVY),1280*720.
the CSI0 Sensor Configuration Register value: CSI_SENS_CONF = 0x00009A00 (External VSYNC mode ,UYVY , 10BIT_DATA_WIDTH,Sensor Protocol:Gated clock mode)
any idea about dealing with this problem?
thank a lot!
Hi lin
one can try to reuse adv7180 driver an check below
https://community.nxp.com/docs/DOC-332679
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
The issue was done!The data pin must to connect data 12 -19,if using yuv 8bit format camera!