Hi !
I made a board according to the layout of the imx8mm EVK SOM board. After I got it, I tried to download the u-boot firmware, but I got the following serial port printing information:
U-Boot SPL 2018.03 (Nov 16 2021 - 20:11:06 +0800)
power_bd71837_init
DRAM PHY training for 2400MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training FAILED
DRAM PHY training for 400MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DRAM PHY training for 100MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DRAM PHY training for 2400MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training FAILED
Then there is nothing left.
By positioning, I found that it was stuck in a memset() function in the board_init_r() function. So how can I solve it?
Should I use mscale_ddr_tool? But the layout is according to the EVK board. I don't know...
Please help me in this case.
Thanks!
Hi
yes, recommended to run ddr test and update image according to i.MX 8M Family DDR Stress Test User Guide
Best regards
igor
I have used v15 script to run the ddr test according to i.MX 8M Family DDR Stress Test User Guide, and this is the log:
Downloading file 'bin\ddr4_train1d_string_v201709.bin' ..Done
Downloading file 'bin\ddr4_train2d_string_v201709.bin' ..Done
Downloading file 'bin\ddr4_imem_1d_v201709.bin' ..Done
Downloading file 'bin\ddr4_dmem_1d_v201709.bin' ..Done
Downloading file 'bin\ddr4_imem_2d_v201709.bin' ..Done
Downloading file 'bin\ddr4_dmem_2d_v201709.bin' ..Done
Downloading IVT header...Done
Downloading file 'bin\m845s_ddr_stress_test.bin' ...Done
Download is complete
Waiting for the target board boot...
===================hardware_init=====================
********Found PMIC BD718XX**********
hardware_init exit
*************************************************************************
*************************************************************************
*************************************************************************
MX8 DDR Stress Test V3.20
Built on Feb 23 2021 13:54:04
*************************************************************************
Waiting for board configuration from PC-end...
--Set up the MMU and enable I and D cache--
- This is the Cortex-A53 core
- Check if I cache is enabled
- Enabling I cache since it was disabled
- Push base address of TTB to TTBR0_EL3
- Config TCR_EL3
- Config MAIR_EL3
- Enable MMU
- Data Cache has been enabled
- Check system memory register, only for debug
- VMCR Check:
- ttbr0_el3: 0x93d000
- tcr_el3: 0x2051c
- mair_el3: 0x774400
- sctlr_el3: 0xc01815
- id_aa64mmfr0_el1: 0x1122
- MMU and cache setup complete
*************************************************************************
ARM clock(CA53) rate: 1800MHz
DDR Clock: 1200MHz
============================================
DDR configuration
DDR type is DDR4
Data width: 32, bank num: 8
For DDR4, bank num is the total of 2 bank groups and 4 banks per group
Row size: 16, col size: 10
One chip select is used
Number of DDR controllers used on the SoC: 1
Density per chip select: 2048MB
Density per controller is: 2048MB
Total density detected on the board is: 2048MB
============================================
MX8M-mini: Cortex-A53 is found
*************************************************************************
============ Step 1: DDRPHY Training... ============
---DDR 1D-Training @1200Mhz...
[Process] End of initialization
[Process] End of read enable training
[Process] End of fine write leveling
[Process] End of read DQ deskew training
[Process] End of MPR read delay center optimization
[Process] End of Write Leveling coarse delay
PMU: Error: Dbyte 3 lane 0 txDqDly passing region is too small (width = 0)
PMU: ***** Assertion Error - terminating *****
[Result] FAILED
I'm very confused, because I made this board according to the EVK board files, please help me....
Thanks!!!
from log "Dbyte 3 " you can recheck board layout for this part. In particular
Step5. Switch to worksheet tab “BoardDataBusConfig” to check data bus assignment.
MSCALE_DDR_Tool_User_Guide.pdf
Best regards
igor
sorry tab “BoardDataBusConfig” is for LPDDR4. Regarding error in step 2, from log:
Data read was : 0x0000000040001890
But pattern was : 0x0000000040000080
one can check layout (probably there are errors) and check signals with oscilloscope
data bits which are different.
Best regards
igor
Hi!
Today I adjusted the 32-bit ddr4 to 16-bit, (I don’t know if it’s the high 16-bit or the low 16-bit, I didn’t find it in the datasheet)
And I used the ddr-test-tool to test it, it's the result:
Training pass, but the step 2 failed. Please give me some advice. Thank you!
Regards
shaotang